How can we help you today?

Statement of Volatility for APC by Schneider Electric PowerShelf products.

Issue:
Statement of Volatility for APC by Schneider Electric PowerShelf products.

Product Line:
SENVPMC001 – PowerShelf Management Controller
SENVPMC002 – PowerShelf Management Controller for GB300
SENVPS33KB2 – 33 kW, 50 VDC, 1U, GB200 PowerShelf
SENVPS33KB3 – 33 kW, 50 VDC, 1U, GB300 PowerShelf
SENVPS33KL-NP – PowerShelf with PMC included and PSU slots

Environment:
APC by Schneider Electric PowerShelf products listed above where a Statement of Volatility is required for security, data retention, equipment handling, decommissioning, or other applicable compliance requirements.

Cause / Resolution:
A Statement of Volatility provides information regarding the memory and data-retention characteristics of a product. This information can assist organizations in evaluating equipment where cybersecurity, information security, data handling, redeployment, decommissioning, return, disposal, or other applicable security requirements need to be considered.

The Statement of Volatility applicable to the PowerShelf products listed in this FAQ is provided as an attached document.

Customers should review and download the attached Statement of Volatility for the detailed information applicable to the covered PowerShelf products, including the applicable memory components and data-retention characteristics documented for the products.

Important:
The attached Statement of Volatility should be used as the primary reference for the products covered by this FAQ. Confirm that the applicable product SKU is listed as covered by the document before using the Statement of Volatility for security, compliance, decommissioning, equipment transfer, or data-handling requirements.

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Saudi Arabia

Attachment(s)
PowerShelf_SOV_V1_Nov_12_2026.pdf [127.04 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation