How can we help you today?

Aveva Plant Scada 2023 R2 - How to setup Plant SCADA to be an OPC UA server to third party OPC UA client.

Issue:

How do we setup Plant SCADA to be an OPC UA server?

Product Line:

Aveva Plant SCADA 2023 R2.

Resolution:

Here is a quick setup process to guide you with setting up Plant SCADA as an OPC UA server.

1.      Run the Computer Setup Wizard and confirm on the Network Model page that networking is enabled. This is required even if you are running the OPC UA Server and the Plant SCADA server on the same computer.

Network model page

2.   In the Configurator, configure the Runtime Manager to run as a Service.

Runtime Manager to run as a Service

3.      Enable Encryption on the Plant SCADA Server hosting the OPC UA Server.

Enable Encryption

4.      Configured the Plant SCADA OPC UA Server with the Security policy as needed. Note the Endpoint URL as it will be required when configuring the connection in the OPC UA client.

Security policy

5.      Confirm the Configurator settings for the OPC UA Server and close the Configurator.

6.      Configure OPC UA Client to connect with the Plant SCADA OPC UA server (using UAExpert as an example).

Configure OPC UA Client

7.   Test and confirm that the connection works and that it is possible to browse for the variables.

UA Expert test client

For more details, please consult the Help in Aveva Plant SCADA 2023 R2.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation