How can we help you today?

EAE26.0: How to display Date & Time on EAE HMI Runtime

This knowledge base article provides a graphic object which was developed in C# to display Date & Time on Canvas of EAE HMI runtime.

This Graphic object can be imported to Ecostruxure Automation Expert 26.0 version only. In case, required to import in upcoming versions, we need to upgrade the project and Export the graphic object. This exported graphic object can be imported on the same version.

  1. Kindly download the graphic object provided with this article and place it on PC where we need to import to EAE project.

2. Now Open the EAE Project and then import the Graphic object as shown below.

y1

3. User can see a popup as shown below, giving information that this graphic object will be added to the solution. Click OK.

y2

4. Now Users can notice that the Date&Time Graphic object has been added under HMI Graphics, as shown below.

y3

5.  Now open the "Open Start Canvas" from HMI Canvases -> select your created resolution, as shown below

y4

6. Drag and drop the Graphic object on to the Start Canvas at Top line where we can see the Date & Time in all canvases in Runtime, as shwon below.

y5

7. Finally Build the project and Start the HMI runtime and user can observe that the Date & Time has been displayed on top header of Canvases.

y6

Schneider Electric Saudi Arabia

Attachment(s)
DateTime.20261008-105943370.graphic.zip [5.82 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation