How can we help you today?

Is it possible to monitor the Primary and Standby PLC state of the M580 redundant system via the Ecostruxure OPCUA Server Expert?

Issue:

Monitoring the Primary and Standby PLC state of the M580 HSBY system via the Ecostruxure OPCUA Server Expert 2.1.4906 SP3


Product Line:

Ecostruxure OPCUA Server Expert


Resolution:

Yes, it is possible via the "#DeviceServiceLevel computation" option in the OPCUA Server Expert configuration. To enable, launch the configuration tool and go to the "communication"  settings and check the "Extended rules" .

image2

image1

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation