How can we help you today?

What termination resistor is recommended for a PM800 device that concludes a Modbus daisy chain configuration?

Issue
Customer would like to know the appropriate termination (End-of-Line) resistor to use with a PM800 when it is the final device in a 2-Wire RS-485 daisy chain.

Product Line
Schneider Electric PM800 Series (PM800, PM820, PM850)

Environment
Hardware - Modbus Communication: Installation/Configuration

Cause
Documentation regarding the appropriate termination (End-of-Line) resistor may be difficult to locate.

Resolution

Use part number MCT2W when a PM800-series meter is the final device in a 2-wire RS-485 daisy chain. The MCT2W is an RS-485 line terminator specifically designed for 2-wire daisy-chain communications.

For PM800 Documentation, please see attached user guide.

Schneider Electric Saudi Arabia

Attachment(s)
PM800 User Guide.pdf [3.42 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation