Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Do ATV320 Drives have Real Time Clock built-in?
Issue:
Real Time Clock built-in on the ATV320.

Product Line:
ATV320

Environment:
All

Cause:
Need time stamp on Faults

Resolution:
No, ATV320 drives do not have Real Time Clock in them. Therefore, there is no Time Stamp in the Fault History.