Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Control Expert 15 returns error 'mfc140u.dll is missing' when starting
Control Expert returns the error 'system error: mfc140u.dll is missing' when trying to start.

This error will occur if the mfc140u.dll file already exists on the PC and it is of a newer version when Control Expert is installed.  The 'mfc140u.dll' file is part of the 'Microsoft Visual C++ 20xx Redistributable ' libraries that gets installed during the Control Expert installation process.  Per Microsoft rules, a software installation is not allowed to overwrite an existing version of a Microsoft '.dll' with an older version.  This rule prevented the
proper installation of the required  'Microsoft Visual C++ 20xx Redistributable ' libraries.

image.png


The specific version 'mfc140u.dll' file is essential for the registration of other '.dll's that are included with Control Expert.  As a result of this, the error could also be accompanied with the following error:

image.png

To resolve the issue,
  • Rename the existing .'mfc140u.dll' file.
  • Uninstall Control Expert.
  • Reboot the PC.
  • Reinstall Control Expert.