Auxiliary contact block with references LAG8N113P & LAG8N203P, can be fitted either on the right lateral face or the left lateral face of the contactor. Means, these auxiliary contact blocks can be fitted on the 1st left for 1st right position of the contactor.
LAG8N113 & LAG8N203 Auxiliary contact blocks, can be installed at the 2nd left or at the 2nd right position of the contactor.
Note: The same reference auxiliary contact block(s) can be fitted to the right or left side of the contactor.
LAG8N113 & LAG8N203 Auxiliary contact blocks, can be installed at the 2nd left or at the 2nd right position of the contactor.
Note: The same reference auxiliary contact block(s) can be fitted to the right or left side of the contactor.
Publicerad för: Schneider Electric Sverige