Issue
M340 to M580 conversion with Device DDT's
Product Line
Modicon M340
Modicon M580
Environment
UMAC
EcoStruxure Control Expert
Resolution
Unfortunately the UMAC tool is not there yet. When using State RAM in the M340 the UMAC will put the modules in as topological then create an ST section to move the topological addresses to State RAM addresses. If you used topological addressing in the M340 project, the topological addressing will stay.
Publicerad för: Schneider Electric Sverige