Problem: In some cases, there may be a mismatch between the actual RBC Serial Number and the RBC Serial Number reported through the NMC:

Product Line: Smart-UPS SRT 1-3kVA with Serial Number date codes earlier than AS2415
Cause: The RBC Serial Number is programmed into the UPS during manufacturing for UPS units manufactured before week 15 of 2024. If the RBC is replaced, this can lead to a situation where the actual RBC Serial Number and the RBC Serial Number reported through the NMC are different. This value is not user configurable.
Resolution: The RBC Serial Number is no longer programmed into UPS units manufactured after week 15 of 2024.
Product Line: Smart-UPS SRT 1-3kVA with Serial Number date codes earlier than AS2415
Cause: The RBC Serial Number is programmed into the UPS during manufacturing for UPS units manufactured before week 15 of 2024. If the RBC is replaced, this can lead to a situation where the actual RBC Serial Number and the RBC Serial Number reported through the NMC are different. This value is not user configurable.
Resolution: The RBC Serial Number is no longer programmed into UPS units manufactured after week 15 of 2024.
Yayımlanma amacı: Schneider Electric Turkey




Yardıma mı ihtiyacınız var?
Ürün seçici
Uygulamalarınız için doğru ürünleri ve aksesuarları hızlı ve kolay bir şekilde bulun.
Teklif Alın
Satışla ilgili sorularınızı çevrimiçi olarak başlatın, bir uzman sizinle bağlantı kuracaktır.
Satış noktaları
Konumunuza en yakın Schneider Electric distribütörünü kolayca bulun.
Yardım Merkezi
Tüm ihtiyaçlarınız için destek kaynaklarını tek bir yerde bulun.