我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How is the motor power scaled on an ATV61 / ATV71 analog output?
Issue:
Scaling of motor power on ATV61 / ATV71 AO1.

Product Line:
ATV61

Environment:
Analog output

Cause:
n/a

Resolution:
It is scaled from 0 to 2.5 times the Rated Motor Power (nPr), as set in the Simply Start or Motor control menus.