Issue
How do I connect a 940-1500 extension cable to my existing serial cable?
Product Line
- UPS Interface Cables
- AP9815/940-1500
Environment
- Users needing to extend the length of serial connection to the UPS
- UPS models with a DB-9 serial port
Cause
AP9815 or 940-1500 does not replace any interface cable packaged with PowerChute software or offered separately. It is simply an extension cable to extend the connection between a computer and APC UPS with a DB-9 port for communication purposes..
Resolution
APC SKU: AP9815
APC Part Number: 940-1500
Length: 15 feet
This cable must be plugged directly into the computer interface port of the UPS. No more than one can be used at a time. This cable is a highly shielded, straight, pass-through interface cable. It is designed to be used in conjunction with the standard six foot PowerChute interface cables, i.e. those cables with APC part numbers 940-0020, 940-0023, 940-0024 and 940-0024.
發佈於:施耐德電機Taiwan