我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: What is a good source of information for crossing over an AC variable speed drive or soft starter?
Issue:
Looking for a good source of information for crossing over an variable speed drive or soft starter?

Product Line:
AC Drives and Soft Starters

Environment:
All

Cause:
Drives and soft starters Cross reference

Resolution:
Reference the AC Drives and Soft Starts Pricing Guide document  8800PL9701 or Substituting variable speed drives guide both are attached.
Please note that when cross referencing drives there are several things to consider.  Application, motor type (VT or CT), enclosure size, heating, control of the drive, installation location.

Please visit the following website for product selection: www.altivardrives.com



For additional assistance with a drive selection or cross, please contact the local Field Sales office or the local PAE - Product Application Engineer.

https://www.se.com/download/us/en/details/3449414-Substituting-oldnew-variable-speed-drives/?reference=60962-EN

施耐德電機Taiwan

附件
ATV Old-New Substitution Guide.pdf [114.08 KB]
product family replacements.pdf [71.07 KB]
Schneider-ATV31-ATV312-Replacement.pdf [126.88 KB]