我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the I/O Expander’s Digital Inputs and Outputs function if the power supply is not connected?

In the I/O expander, only the Analog Outputs are excited by the internal power supply. Digital Inputs and Outputs are externally excited and powered from the meter itself. So, Digital Inputs and Outputs will work without the power supply being energized.

Last Revised: April 9, 2008
Applies To: ION 8600, I/O Expander
Original Author: KG
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191645 V1.0, Originally authored by KBAdPM on 04/10/2008, Last Edited by KBAdPM on 04/10/2008
Related ranges: Cabling and connection accessories, ION8600