我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why does the Quantum Unity PLC (140CPU43412A) timer reset on a power cycle?

The timer resets on a power cycle because the customer has made a Project Backup. When a Project backup is made, every power cycle
will cause a cold restart (%S0). This cold restart will reset all timers.