我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is a NW-BM85-000 Modbus Plus to Modbus Bridge Multiplexer considered a DTE or DCE device?

The NW-BM85-000 Bridge MUX is considered Data Terminal EQUIPMENT (DTE) device. Modems are Data Communication EQUIPMENT (DCE). A modem cable must be used when connecting the bridge to the modem.
The following list identifies the type of cable and naming convention used to connect to different types of EQUIPMENT.

DTE - DCE: Modem Cable or Straight Through Cable
DTE - DTE: Null-Modem Cable (crossed cables)
DCE - DCE: Tail Circuit Cable Interface Mechanical


Legacy KB System (APS) Data: RESL1346 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modbus