Issue
What is the difference between the SyMax Model 50 programmable controllers 8005CP50 and 8005CP51?
Product Line
SyMax
Environment
8005CP50
Resolution
The difference between the two SyMax Model 50 programmable controllers is the power voltage rating.
8005CP50 is a 120/240 VAC Processor Unit.
8005CP51 is a 24 VDC Processor Unit.
發佈於:施耐德電機Taiwan