Issue
What is the difference between the 8020SCP424 and the 8020SCP444 SY/MAX controllers?
Product Line
SY/MAX
Environment
8020SCP424
Resolution
The difference between the 8020SCP424 and 8020SCP444 SY/MAX controllers is the memory type utilized. Both units have 16K of user RAM; however the 8020SCP444 also offered 11K of nonvolatile memory for program storage on UVPROM.
發佈於: 施耐德電機Taiwan