我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can I monitor a Standby unit in a Quantum Hot Standby system using SNMP?

Yes. SNMP service is active on an NOE771xx module operating in a Quantum HSBY.The last octet of the Standby address
will be offset by +1 from the Primary.. Primary address of 192.168.100.1 will result in a Standby address of 192.168.100.2