我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to Add a '.dat' formatted loadable to ProWORX Nxt

Issue
How to add a '.dat' formatted loadable t 'ProWORX NxT'

Product Line
'ProWORX NxT'

Environment
Windows 7, 10

Resolution
The following steps can be used to add a custom loadable (e.g. EUCA loadable, etc.) that is in the form of '.dat' to
a '.ProWORX NxT' project.

  • Click on 'Configuration\Configuration'.
xc v
  • Click on the 'Loadable Library' tab.
  • Select 'Modicon' in the 'Source of Loadables' section of the 'Loadable Library' tab.
  • Click on Browse:
df
  • Select the 'EUCA-8.dat'.
  • Click on OK
fgt
  • Click on Transfer.
dfgh
  • Browse for the 'PROWORX.USL'.
  • Click on OK.
fdgh
  • Click on the "User Loadables' tab.
  • Select the 'EUCA' loadable to select it..
  • Click on the 'Load' button to add the loadable into the project database..
  • Click on 'OK' to close the 'Controller Configuration' window.
dfgh