我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the screw size and wire sizes for the CT and PT terminal connections on the CM4000 series meters?
Issue
What are the screw size and wire sizes for the CT and PT terminal connections

Product Line
CM4000
CM4250
CM4000T

Environment
Hardware Specifications

Resolution
The terminal screws are 4mm with a 0.7 pitch. Each meter is supplied with spade lugs that accommodate 10-12 AWG wire.