搜尋常見問題
What does AMPS OVER represent on the display of an Energy Meter?
Issue
AMPS OVER displayed on Energy Meter
Product Line
EMBxxxx, EMExxxx, EMHxxxx
Environment
Front panel display
Resolution
If the measured current is greater than 110% of the rated CT range, the display will show AMPS OVER and indicate the specific phase(s).