我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can a 3710 ACM meter have a Direct Delta connection at 600VLL?

No, a 3710 ACM meter cannot be setup for a Direct Delta connection at 600VLL. The maximum applicable voltage for a delta connection in a 3710 ACM is 120VLN / 208VLL, therefore, PT installation is mandatory in order to use the Delta volts mode in a 3710 ACM for 600VLL.

Last Revised: November 22, 2007
Applies To: 3710 ACM
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189563 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: 3710 ACM