我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Knockout punches used for the DIN Standards for ION meters

Knockout punches are used on switchgears to clear the DIN holes to attach meters. Knockout punches suitable for ION devices are carried by and found at a company called Grenlee. Please see the company's website at http://www.mygreenlee.com
------------------------------------------------------------------------------------
Last Revised: April 18, 2007
Applies To: ION 6200, 7300 / 7330 / 7350, 7550 / 7650
Original Author: KG
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191716 V1.0, Originally authored by KBAdPM on 04/19/2008, Last Edited by KBAdPM on 04/19/2008
Related ranges: ION7550/ION7650, ION7300, ION6200