我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ION7650 or ION7550 meter gives Error 195 on the front panel

Issue
Error 195 appears on the front panel of an ION7650 or ION7550 meter

Product Line
ION7650

ION7550

Environment
HMI of meter

Resolution

If Error 195 appears on the front panel of an ION7650 or ION7550 meter, upgrading the firmware to version (v352) or later will resolve this issue.