我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the new 140NRP95400 or 140NRP95401C Fiber Optic Repeater be added into Concept I/O Map
No.
The 140NRP95400 and the 140NRP95401C Fiber Optic Repeater only requires power from the Quantum rack.
There is no communication over the back plane between the repeater and the other modules in the rack.