我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the frame sizes of ATV61 and ATV71 drives?
Issue:
Frame sizes for ATV61 and ATV71

Product Line:
ATV61 ATV71 Altivar drives

Environment:
All

Cause:
n/a

Resolution:
See Attached Chart and use the Engineer Frame column based on the part number of the drive.

施耐德電機Taiwan

附件
Frame sizes atv61_71_framesizes_iv.xls [29 KB]