我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can I check fault time on an Altivar 61/71 Drive?

Issue:
ATV61/71 Fault time check

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
Fault time

Resolution:
The drive does not have a real time clock to show fault time of the day.  It will only show you the drive's elapsed time during the fault.  You can then compare to the 'Run Time' shown in the Drive Menu under 1.2 Monitoring.
To navigate to Fault History:
Go to Drive Menu > 1.10 Diagnostics > Fault History