Power Monitoring Expert 7.2 - Why doesn't 'Update OPC Server' work when run on an Engineering Client machine?
When the Management Console is run on an Engineering Client machine, the 'Update OPC Server' option is available. However, if this option is chosen, it fails with an error dialog.
'Update OPC Server' should not be available on an Engineering Client machine. This will be corrected in a future release. 'Update OPC Server' must be invoked from the Primary server.