我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How do you program the customer enclosed drive to follow speed pot in hand and auto modes?

Issue:
Programming drive to follow the speed por in hand and auto modes.

Product Line:
M-flex, E-flex etc

Environment:
All

Cause:
They do not have a separate 4- 20mA speed signal for auto mode so they want to use the speed pot mounted on the enclosure in auto mode.

Resolution:
Programming changes as follows
Main menu
Set access level to Expert

Drives menu
Menu 1.6
Ref 1 - AI1
Ref 2 switching is channel 1 active

Menu 1.7
Ref switching LI3
Ref 1b switching is AI1