Issue:
SCF is a Short Circuit Fault
Product Line:
ATV58, FLEX58
Environment:
All models and serial numbers
Cause:
Possible causes are:
1. heat sink fans are not operating
2. The output transistors (IGBT) are not gating correctly
3. Short circuit in the motor or motor wiring
4. capacitance due to long motor lengths
Resolution:
1. replace the heat sink fans
2. repair or replace the drive. This drive has been discontinued. Parts may not be available.
3. check motor for shorts, Megger motor and motor wires with minimum of 1000v megger
4. add a load filter
發佈於:施耐德電機Taiwan