我们今天能为您提供什么帮助?

Where can I find the flange kit part numbers for the ATV61 and ATV71 drives?

Issue:
Where can I find the flange kit part numbers for the ATV61 and ATV71 drives?

Product Line:
ATV61, ATV71

Environment:
All serial numbers for ATV61

Cause:
N/A

Resolution:
e

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)