我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What can cause an INF1 (Rating Error) on an ATV61 or ATV71 drive?
Issue:
Causes for INF1 (Rating Error) on an ATV61 or ATV71

Product Line:
ATV61/ATV71 drives

Environment:
INF1 faults

Cause:
n/a

Resolution:
Check the part number of the power board. Check the graphic terminal the size and the voltage of product. Check the power identification number.