我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What do you do with the DC choke on an ATV61 or ATV71 high horse power drive when mounting a flange kit?
Issue:
Mounting an ATV61 with DC choke and a flange kit.

Product Line:
ATV61 ATV71 HHP Drives

Environment:
All serial numbers for ATV61 and ATV71 Drives

Cause:
N/A

Resolution:
When using the flush mount kit, the manual for the drive advises removing the dc chokes from their chassis and mounting them directly to the back pan of the enclosure.
See attachment.

施耐德電機Taiwan

附件
Flange Mounting with heatsink outside the enclosure.png [320.15 KB]