{}
搜尋常見問題
EEM Trend Report columns are alphabetized when report is generated
Issue
User has configured Trend Analysis in data groups to show the graphs with stacked columns in a particular order. When the Trend is saved as Report and generated the report columns are alphabetized.

Product Line
ION EEM 5.x

Environment
ION EEM 5.x
Reporting Tab Web user interface

Cause
The Trend and Report graphs show the stacked columns as the user configured; however, the generated report columns are now alphabetized.
Trend Report table
Report output

EEM development team has captured this as new request to be evaluated.
A possible workaround would be to export the Report into an Excel format and edit the spreadsheet.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: