我们今天能为您提供什么帮助?

PlantStruxure PES [V4.0]: How can I change the ports used by the system server?

Goals and Symptoms

Adjust ports used by the system server


Facts and Changes

PES version V4.0


Causes and Fixes

You can configure the port that is used by the system server for client/server connection in the System Server Configuration Wizard.

Please refer the below image for changes in the System server Configuration Wizard

System server Configuration wizard

Please refer the below images for changes in the Engineering client Configuration wizard

Engineering client configuration wizard
Before changing the port, run netstat -ano in a command prompt on the PC on which the system server is installed. This command lists the ports that are currently in use on the PC.
Verify that the port that you want to use is not already in use.

If you change the port from its default value (TCP port 9950), you need to configure the same value for each engineering and operation client that connects to the server by using their respective Configuration Wizard.