我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are the VW3A1101 stored files lost if the HMI is disconnected from a drive?
Issue:
VW3A1101 stored files in the HMI.

Product Line:
ATV61  ATV71

Environment:
All

Cause:
Would like to transfer files

Resolution:
No.  The files that are stored in the HMI remain intact when the HMI is disconnected from the drive.