ATV-IMC" is always 00:00 01/01/2000 | 施耐德電機Taiwan" />

我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Time in ATV71 keypad under "DriveMenu -> ATV-IMC" is always 00:00 01/01/2000
This is because time is not synchronised between ATV71 and IMC card.

To enable time synchronisation the following program line should be added to ATV_IMC_Start POU:
DriveFaultDatation(Activate:=TRUE );