我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: Where is the enter or ENT button on the Altivar ATV61 and ATV71 drives when using the VW3A1101 HMI for programming?
Issue:
ENT button on ATV61/ATV71 when using the VW3A1101 HMI

Product Line:
Altivar ATV61 and ATV71 or any drive using the VW3A1101 for programming.

Environment:
All

Cause:
Need to know how to save the parameters after entering data into the drive.

Resolution:
The enter or ENT button is the large round knob on the W3A1101 keypad. Just push the wheel to enter.