我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to determine the logic input assignments on an ATV61/71 drive?
Issue:
Logic input assignments on an ATV61/71 drives

Product Line:
ATV61/71

Environment:
All products of ATV61/71

Cause:
N/A

Resolution:
Logic input assignments can be viewed by going into the IO map
Drive Menu ~> 1.2 Monitoring Menu ~> IO Map ~> Logic Input Map
Move the cursor over to desire logic input and hit enter to view its assignment.
This same Logic Input map shows the current state of the logic input.