我们今天能为您提供什么帮助?

How to configure the IOScanning table to a 140NOE77101 exchanging with a 140NOC77711 ?

By default the Unit ID value on 140NOE77101’s IO Scanning table is 255. Keeping this configuration it is impossible to READ or WRITE data inside a PLC application through a 140NOC77111.
It is mandatory to change the Unit ID value from 255 to 1 on 140NOE77101’s IO Scanning table.