{}
搜尋常見問題
How are the vertical mounting rails oriented (left / right) in the NetShelter cabinets?
Issue:
When purchasing a replacement vertical mounting rail it's important to know the difference between a Left Hand rail and a Right Hand rail.

Product Line:
NetShelter SX, SV, VX

Environment:
All versions and serial ranges.

Cause:
The part description of the rails read "Left Hand" or "Right Hand", but doesn't specify front or rear.

Resolution:
Please see attached file.

施耐德電機Taiwan

附件
20150911 Mounting Rail Orientation.pdf [22.9 KB]
探索更多
系列:
可能有幫助的文章
探索更多
系列: