我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Where is the ATV61/71 analog input map found?
Issue:
Analog input map location for the ATV61/71.

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Need to verify analog input signal

Resolution:
Analog input signals can be viewed in the VFD.

Navigate to the following and select:
From Main menu
Scroll down to Drive menu and press enter
Select 1.2 Monitoring and press enter
Then choose I/O map and press enter
Scroll down to select Analog Inputs Image and press enter