我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
MiCOM relays. Specific timers related to the user interface in the MiCOM Px2 relays.
Follwowing timers are fixed in the Px2 relays.
  • LED refresh time is 500 ms
  • LCD refresh time is 1 s
  • The password confirm info display time delay is 2 s
  • Programming mode timer after login to the front panel is 5 min. During this time the relay will not accept to change any settings from remote. It is considered as 5 min of inactivity.