我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can I identify a drive part number inside an 8839MFD?

Issue:
Identification of drive part number inside an 8839MFD.

Product Line:
8838 MFD  MFLEX

Environment:
All

Cause:
Need replacement

Resolution:
Check the enclosure name plate on the door interior for the power converter number also the drive number.
If the drive an be powered go to the identification menu (Main menu, Drive menu, Identification menu) drive number will be listed.
Consult the 8839 MFlex manual for complete details.