我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
I updated the time of my CPU with the time of my PC, and I see a difference between the two.
The PC doesn't manage the automatic adjustement clock for the daylight saving time.
In Windows®, set the option "Automatically adjust clock for daylight saving time".