搜尋常見問題
What is the part number of the cable that connects to a Lexium 32x drive from a PC?
Issue: Part number
Product Line: Lexium 32x
Environment: None
Cause: Maintenance
Resolution: The part number of the cable connecting a PC to a Lexium 32 drive is TCSMCNAM3M002P,
A brief description of the cable is given below.
Product Line: Lexium 32x
Environment: None
Cause: Maintenance
Resolution: The part number of the cable connecting a PC to a Lexium 32 drive is TCSMCNAM3M002P,
A brief description of the cable is given below.
發佈於:施耐德電機Taiwan
這是否有幫助?
探索更多