我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the braking capacity of the ATV312HU15N4?
Issue:
Braking capacity ATV312HU15N4

Product Line:
ATV312

Environment:
All

Cause:
Braking capacity ATV312

Resolution:
Without a braking resistor, it is 50% of nominal motor torque. With braking resistor, it is 100% of motor torque continuous and 150% of torque for 60 seconds.