我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the Unity Momentum PLCs support a Modbus Function Code 22 (16 Hex) Mask Write 4X Register request?
Issue:
Does the Unity Momentum PLCs support a Modbus Function Code 22 (16 Hex) Mask Write 4X Register request?

Product Line:
Momentum

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
Yes. The New Unity Momentum processor does support Function Code 22 (Mask Write 4X Register). This Modbus/TCP messaging command is supported only with the Momentum acting as a Server and responding to a Function Code 22 request from any 3rd party controller or a SCADA.