我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
M580 - Why the EFB "Drop" doesn't work in M580 with Quantum EIO architecture?
Question:Why the EFB "Drop" doesn't work in M580 with Quantum EIO architecture? all the channels display "0", no any data can be read:


Answer: The version of M580 CPU need to equal or later than 2.10, then the function will be correct.